This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25981: Parallel Connection for Higher Current

Part Number: TPS25981
Other Parts Discussed in Thread: TPS25982

Tool/software:

Hello experts,

I am planning to use TPS259814ARPWR on my board to to protect against high current.
The LOAD current is about 12A and I have to set the protection when the current is >=14A.

Since the TPS259814ARPWR max current limit is 11A, I was wondering if I can set two TPS259814ARPWR in parallel.
Each device set on 7A, giving 14A in total.

Is this configuration possible?

Best Regards,
Filipe