This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088MH-2EVAL: Unable to find Detailed Guide on Calculating Compensation Network

Part Number: LM5088MH-2EVAL
Other Parts Discussed in Thread: CSD18534KCS, LM5088

Tool/software:

Hello everyone,

I’m currently working on designing a compensation network for the CMC buck converter LM5088-2.

However, I’ve been struggling to find a detailed and clear guide for calculating the compensation components (Rcomp, Ccomp, and CHF) (poles and Zeros)

Im interested to see the stability of the converter loop and tune the system for the application.

While the datasheet and the provided calculation tool (Quickstart.xls) are helpful to some extent, they lack the detailed steps and explanation I need to fully understand and implement the design.

I would greatly appreciate it if anyone could share a suitable document, solved examples, or any additional resources that provide a step-by-step explanation for designing the compensation network specific to the LM5088-2.

The design specs I'm working on are:

Vin Min : 18V

Vin Nom : 27V

Vin Max : 31V

Vout : 15V

Iout : 5A

Fsw : 250KHz

L : 47uH

Rsen : 20mOhms

Cout : 500uF

Mosfet : CSD18534KCS

Diode : STPS30M60ST

Rramp : 154Kohms

Cramp : 1.2nF

Cboot : 0.1uF

Thanks in Advance,
Arvind