Tool/software:
I am building a low-power solar energy harvesting circuit using the BQ25570. It seems to work, but I am wondering if I am seeing the expected behavior from the MPPT. Every 16s it samples the open circuit voltage, as expected, and then it adjusts the charging current, but only a little bit - say enough to change the loaded input voltage by 10 mV. It seems to converge, slowly, to a charging current of ~1.5mA, which is appropriate given the low input energy. Is this how the part is supposed to behave? There is little information in the datasheet about how MPPT is implemented. Thanks!