Other Parts Discussed in Thread: LM3310, LM2700,
Tool/software:
Vin = 3.3
Vpos = 15
Vneg = -15
Ipos = 0.1
Ineg = 0.1
Using the equations in the datasheet I get:
I_Lp = 710mA
I_Ln = 870mA
L1 = 14uH
L2 = 12uH
However, using the Webench Power Designer I get:
I_Lp = 196mA
L1 = 4.7uH
It seems the equations in the datasheet are wrong because even for a relatively low current of 100mA I end up with very large inductors.