Tool/software:
Hi Team,
I have used the active clamp forward topology with interleaved configuration for 250W output (In interleaved each section can source 125W) boost converter design.
Design requirements are listed below
Input voltage range : 12-36V typical 28V - As design calculation during 12V operation input current will be 13A in single section and 26A for both the section.
Output : 250W (Voltage 50V & Current 5A) - Since it was interleaved design Each section can source 50V @ 2.5A (125W).
Step-up transformer turns ratio: 1:5
SWT frequency: 500KHz
Design considered Efficiency : 91%
Power loss for this design calculated around 15W (Calculated for Primary Switching MOSFET, Clamping MOSFET, Transformer, secondary side rectification MOSFET and switching inductor)
Now issue is the clamping P-CH MOSFET getting degraded and it leads component failure during output load test. Since it was design validation I have currently operating single channel alone one more channel gate signals are isolated method.
I have used 2 MOSFET parts listed below both MOSFET's are getting failed 2 times while performing load test (Load current is 0.5A not even loaded full load 2.5A). We could not assume the MOSFET getting failed due to more voltage or more magnetizing current flow or reverse recovery loss.
1) SQS481ENW-T1_GE3 MOSFET P-CH 150V 4.7A 2.57E 62.5W 305pF SMT PowerPAK 1212-8W RoHs - Initial design consideration part having 150V VDS voltage but 4.7A current.
2) SI7113DN-T1-E3 MOSFET P-Ch 100V 13.2A 134mE 52W SMT PowerPAK 1212-8 RoHs - Based on initial design MOSFET failure suspected more current flow dame a device so 13.2A current rating FET replaced with 100V VDS.
As per design magnetizing current is calculated by the below formula
Dmin x Vin_Max or Dmax X Vin_Min / Fsw X Magnetizing inductance = ((12V X 80%) / (500KHz X 46uH) = 0.417A
Also calculated power loss for the clamping MOSFET are conduction loss, Turn off loss and gate charge loss = 0.64W
My query is apart from this parameters is there any further method is available to calculate the power dissipation....?
What are the possibilities to degraded the clamping FET...?
Is there any other method to find out magnetizing current calculation....?
Regards
Prasanna