This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76002: Application issues.

Expert 2020 points
Part Number: LM76002
Other Parts Discussed in Thread: LMR51635,

Tool/software:

Hi Team,

Need to make a BUCK power supply, input DC 18~60V, output 24V, current 0.8~1.5A
Can LM76002 or LMR51635 be implemented?
1. What should be noted about loop compensation?
2. What is the output state when the voltage is below 24V, such as 20V?
3. Which has greater heat loss between LM76002 and LMR51635? What are the differences in PCB layout? What is the difference between EMI?

Thx!