This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: Parameters of peripheral components when output power is 60W with 200V unsuppressed load dump protection circuit

Part Number: LM7480-Q1

Tool/software:

Hi team,

The datasheet covers 200-V Unsuppressed Load Dump Protection Application with output power of 25W. In customer's use case, output power is 60W(24V2.5A). How should my customer choose the parameters of peripheral components such as input capacitors and output capacitors and so on? The selection of MOSFETs is stated on the datasheet, so no need to confirm.

Best regards,

Shunsuke Yamamoto