Can the TPS40077 be used with a 12V input and generate -4V @ 10A? Based on the inverter reference design it is possible to generate a -5.2V @ 4.5A. The datasheet for the device also says it supports up to 20A. The TPS40077 was not loaded in SwitcherPro so I was not able to determine if this was beyond the spec of the device. If this is possible, can you please recommend a sample circuit diagram for this implementation?