This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22963C: spec check

Part Number: TPS22963C
Other Parts Discussed in Thread: TPS22991

Tool/software:

Hi 

Could you help confirm the following specifications. Does TI have -55~125°C specifications to recommend?

Thanks ** Mainly P2P, if there is no P2P with the same function, please recommend it, thank you

TPS22963CYZP

TPS22992RXPR

  • Hi Gareth,

    Since these devices are not made for -55C temperature operation, char is also not done at that temperature and we won't be able to provide the requested data.

    I am double checking if TPS22991 is -55C part.

    Best Regards,
    Arush.