Other Parts Discussed in Thread: REF102, REF70, REF54
Tool/software:
Hi,
I want a very stable precision current source for JFET tail biasing. The current source should have a positive temperature coefficient to cancel out the negative temperature coefficient of JFET gm.
The current rating is 4 mA.
Also please note that entire design operates on +/- 15V, so tail current source will have it reference connected to -15V rail.
Also noise is very important, so the noise addition should be very low, in few fA.
Please suggest me a good way to achieve this. I look forward to hearing from you soon.