This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Considering the need to programm the bq25180 by I2C bus. I understand that any time the device is reset it must be programmed by the controller. Is this right? Or is this programming non-volatile?
In the case we hae the device only supplied by the batterty (Vin disconnected), may the device be programmed by I2C? Or do we always need Vin connectrd to acces the deice by I2C?
Thank you very much in advance.
Regards,
Joel
Hello Joel,
That's correct, memory is volatile and will be lost anytime there is a POR or power is lost.
You can communicate with the charger over I2C with only VBAT present.
Sincerely,
Wyatt Keller
Hello Wyatt,
Thank you.
The device I'm working on will usually be working using the battery. When the voltage of the battery would go down the programmed Vbuvlo value, the bq25180 should automatically disconnect the battery from the system. But it's not clear if the device goes to ship mode with a consumption of nA. What would be the consumption of the bq25180 from the battery in such condition?
This a typical situation when the battery device would be a long time in the shelf and some chip manufacturers call it "shelf mode" for its chargers.
Thank you very much in advance.
Regards,
Joel
Hello Joel,
The BQ25180 disconnects the battery to protect it from deep discharge when the battery voltage drops below the BUVLO falling threshold. At this point, the device is effectively off.
The BQ25180 supports two low-power modes:
I'd also recommend checking out the BQ25188, which we recently released. It's the latest version of the BQ25180 and offers several features and improvements.
Best regards,
Alec Lehman
Hello Alec,
Related to the bq25180. When it disconnects in case of an Undervoltage in the battery, may you please confirm that it will recharge the battery when we will connect Vin power?
Related to the bq25188. In the pdf published it's specified the values of VBUVLO to protect the battery from an undervoltage. But this function is not indicated in the first page of the pdf. I would suggest to include it like it's included in the pdf of the bq25180.
I have to admit that I would be more confortable if the specs of the bq25180/25188 could be included in a standalone device or in a non-volatile configuration.
Regards,
Joel
By the way. May you confirm me that the bq25188 may suply peak currents up to 3Amps from the battery to the SYS output?
Thank you very much in advance.
Regards,
Joel
Hello Joel,
When it disconnects in case of an Undervoltage in the battery, may you please confirm that it will recharge the battery when we will connect Vin power?
Yes, when the battery voltage is below the VBUVLO threshold but above the VBATSC threshold, the battery will charge at the precharge current. The precharge current can be programmed to be either 1x or 2x the termination current, which itself can be programmed to be a percentage of ICHG.
Related to the bq25188. In the pdf published it's specified the values of VBUVLO to protect the battery from an undervoltage. But this function is not indicated in the first page of the pdf. I would suggest to include it like it's included in the pdf of the bq25180.
That's a great point. I appreciate you bringing this up, and we'll consider it for future revisions of the datasheet. Thank you for your feedback!
I have to admit that I would be more confortable if the specs of the bq25180/25188 could be included in a standalone device or in a non-volatile configuration.
We have the BQ25185, which is the standalone (RC-settable) version of the BQ25180. Please feel free to reach out if you have any questions about it!
BQ25185: https://www.ti.com/product/BQ25185
Best regards,
Alec Lehman
Hello Joel,
Yes, the battery overcurrent protection (BATOCP) on the BQ25188 can be set up to 3A. This is an improvement over the BQ25180, which could only set BATOCP as high as 1.5A.
Best regards,
Alec Lehman
Hi Alec,
The bq25185 could be ok, except that it doesn't have the shutdown current of nanoampers that the bq25188 has. The bq25188 looks quite better in terms of shelf mode (when the device has to be stocked in a shelf during a long time).
Thank you very much.
Regards,
Joel
Hello Joel,
Both the BQ25185 and BQ25188 have the 3.2uA ship mode (called factory mode on the BQ25185). One key difference is that ship mode can be exited by a push button press, while the 15nA shutdown mode can only be exited by connecting an input power source to VIN. Additionally, the device registers are not reset when entering ship mode, but they are reset when entering shutdown mode.
Please let me know if you have any questions about either device.
Best regards,
Alec Lehman
Hello Joel,
Understood. Let me know if you have any other questions.
Best regards,
Alec Lehman