Other Parts Discussed in Thread: LMR36506, LMR36006
Tool/software:
Hi team,
Merry Charismas!
My customer use LMR36006AQRNXRQ1 in auto BMS MCU supply, VIN is 24V, VOUT is 5V/60mA. DCDC fail on EMI CE current method and RE (standard :CISPR25 class 4), test result :(CE margin on FM frequency is only 1dB;RE on MW frequency is 2dB above standard) and what they try to do for this result as attachment
They try to change to LMR36006FSCQRNXRQ1 (2.1MHz with SPREAD SPECTRUM), DCDC successfully pass CE(Margin is 6dB) and RE, I also attach what they do for LMR36006FSCQRNXRQ1
But the issue is LMR36006FSCQRNXRQ1 efficiency is too low< 30% at light load 60mA as FPWM, cause thermal issue.
Support need:
- For LMR36006AQRNXRQ1, what else they can do for EMC pass? I confuse EVM test report show 400kHz without SPREAD SPECTRUM can also pass EMI.
- If they change to LMR36006FSCQRNXRQ1, what they can do to improve efficiency, Now inductor is 10uH, I think there is no solution to further improve as datasheet show the same level.
- What other device we can recommend to customer for both good EMC and efficiency(60V Max input, 5V output, <1A is enough)?
BR
Amber