Tool/software:
Hi BU,
Good day!
My customer would like to clarify BATFET_CTRL_WVBUS setting in BQ25628. Could you help to further explain the red box portion? Thanks for the help!
Regards,
John
Tool/software:
Hi BU,
Good day!
My customer would like to clarify BATFET_CTRL_WVBUS setting in BQ25628. Could you help to further explain the red box portion? Thanks for the help!
Regards,
John
Hello John,
Do you have a specific question regarding this bit? The bit's behavior is explained in a couple places within the datasheet, the most thorough section is: 8.3.9 BATFET Control
But there are other sections which explain the bit's impact in other areas of operation as well.
Sincerely,
Wyatt Keller
Hi Wyatt,
Thanks for the response.
I think customer would like to know when assigning 0h for BATFET_CTRL_WVBUS, does this mean allowing BATFET off / system power reset with adapter present?
Customer would like to know what will happen if we assign BATFET_CTRL_WVBUS to either 0h or 1h.
Thanks.
Regards,
John
Hi John,
Please see my explanation below.
As shown in table 8-6 in datasheet section 8.3.9 the BATFET_CTRL_WVBUS bit setting has an impact on IC operation as it pertains to ship mode and system reset functions.
With BATFET_CTRL_WVBUS = 0h and an input adapter connected.
With BATFET_CTRL_WVBUS = 1h and an input adapter connected.
Best Regards,
Garrett