This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: About TPS55289 Inductor

Part Number: TPS55289
Other Parts Discussed in Thread: TPS55288

Tool/software:

Vin:3.2V

Vout : 3.4V+-10%

Vout(max):4.2V

Iout(max)=8A

Vout p-p=+-20mV

A. Assuming the use of Vin 3.3V to convert to Vout 3.4V or 3.1V, is it still necessary to use a 4.7uH inductor? According to Excel calculations, the minimum inductance that can be used is 32.9nH?

B. Can you please confirm if the following circuit settings are correct? Are there any suggested modifications?

Setting:

TPS55289-CALCULATION-TOOL-V1.0 (1).xlsx