This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: BQ25713 I2C address target

Part Number: BQ25713


Tool/software:

Hi TI Forum.

Likely a very quick question to answer, but I have a system with two BQ25713 which I want to be on the same I2C bus.

As I understand the datasheet the BQ25713 has a set I2C address of D6h. However, in the Battery Management Studio, I see a dropdown menu for Tgt Address with D6 (6B) and D4 (6A).
Can I choose between these two addresses to differentiate between the two, or do I need a I2C multiplexer to properly address the two?

The reason I need to address them separately is because I might be in a scenario with my system where one will be in OTG mode and the other receiving power to supply my system and battery.

Thanks in advance.

Kind regards,
Victor Hansen