Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi (sorry -reposting as new question)
Im having issues getting the BQ25895 chip to charge the batteries.
First id like to rule out there is an issue with the schematic, i'm using a custom PCB the schematic is below. We are using two 18650 batteries (in parallel) for charging the batteries we have a solar pane and standard USBC .Please let me know if you see any issues.
Second the registers, Im using a mac so had to install BQstudio via utm and write the registers directly into the firmware. But am i completely messing up these setting? Ive tried just about everything here.
Here are the readings i'm getting after uploading firmware
BQ address = 0x6A
REG0: 0x79
REG1: 0x5
REG2: 0x3D
REG3: 0x3C
REG4: 0x14
REG5: 0x13
REG6: 0x5F
REG7: 0x81
REG8: 0xCB
REG9: 0x4
REGA: 0x93
REGB: 0xA6
REGC: 0x1
REGD: 0x97
REGE: 0x4C
REGF: 0x4E
REG10: 0x7F
REG11: 0x97
REG12: 0x0
REG13: 0xB9
REG14: 0x39
Please let me know, thank you