This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562200: Need Support for RE test issue resolution

Part Number: TPS562200


Tool/software:

Hello,

We are using TPS562200DDC part in our design for the 3.3V generation from 12V input. Max output current on 3.3V is 1.3A. We are doing radiation emission testing and we see that this regulator causes the radiation peak of particular frequencies. 

Below are the radiation peaks we have captured on the scope using near-filed probes in house we do have. 

Can you please help us to here, how we can lower this radiation?