Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ40Z50
Tool/software:
Hello,
I was developing the FW of my master to drive the gauge (v5.04).
The gauge has a 4S (16V) setting, but with a double current (via the TI procedure to go from 30000mA to 60000mA, so calibrating with a factor of 2).
I had several points that I could not resolve (SOH, abnormal T°C on a probe, no FET respond command...), so I decided to do a reset (which did not change anything), then a "shutdown" via the bq studio command.
From this moment on, it is impossible to reconnect to the chip, the gauge is no longer detected, and if I choose the chip manually, the data remains at 0. I spied on the SMBus scope, I can see that the chip does not respond (the bus is neither blocked at 0, nor at 3.3, I have clean signals from the EV2400, so edges, idle state...).
I applied a voltage of 16V on BAT, PACK, VCC to wake up, and also forced these 3 pins to 0 (shunt GND) before restoring the voltage. Note that the cells are glued/soldered, the PCB is sandwiched, so I cannot disconnect VC1, VC2, VC3, VC4 and access to signals.
The commands in bq studio have no effect. No more for FW download.
I don't understand why the chip doesn't wake up
There is no reset pin, so what did I miss?
Regards
CM