Other Parts Discussed in Thread: TPS546D24A,
Tool/software:
1. On TPS546D24A and TPS53681 We do not see option to extract nvm_config_script. Is there any way to get that ?
2.On TPS546D24A and TPS53681 we observed that Few parameters are failing while programming Via PM bus script file.
Further , we tried to manually change few of these registers on TPS546D24A , we were able to do so but same thing when is happening via pmBus programmer script generated by fusion GUI(7.9.1) , it is throwing error and warnings.
For example, Below were failing via script, but we were able to change it when done manual register write.
Warning: config verification for dev 4 at offset 0x2 expect data 0x18, read data 0x17
Error: config verification for dev 4 at offset 0x21 expect data 0xBB, read data 0xCD
config verification for dev 4 at offset 0x21 expect data 0x6, read data 0x6
Also
Similarly for TPS53681 also we observed few errors with current set of programming file.