Tool/software:
Dear Texas Instruments Team,
I am currently working with the TPSF12C1 model in PSpice and have encountered an issue:
When I set the VAMPL parameter to 5V and VOFF of the supply voltage to 0V in the simulation circuit, I do not see any changes in the diagram after clicking "Run PSpice".
This also occurs when I try to connect multiple AC voltage sources in parallel to simulate disturbances.
Could you please advise if there are specific configurations or limitations that I need to consider to simulate these changes correctly?
Thank you in advance for your support!
Best regards,
Tim Evers