This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866S-Q1: PWM Dimming resolution

Part Number: LP8866S-Q1
Other Parts Discussed in Thread: LP8866-Q1

Tool/software:

Hi all

i have a questions regarding the LP8866-Q1 BOOST LED Driver Design Tool.

The image below, which I marked in red, has the Desired LED Dimming Frequency and the Input the PWM Dimming Frequency (The external PWM signal from MCU). Does the PWM input from MCU have to be the same as the desired Dimming Frequency?

for example? if we set the input PWM 244Hz, will the desired PWM Frequency be 244Hz too?

And the other Question from the datasheet, it said that the LED Driver feature 12-bit analog dimming,

what is the different between this:

and how to set the analog dimming?

Thank you