Other Parts Discussed in Thread: TPS25751, BQ25798, TPS65994AD, BQ25750, BQ25756, BQ24140
Tool/software:
Hello,
Could you please recommend a solution for implementing the following project requirements?
- Hardware: Two Type-C PD ports (both sink/source capability) and support for charging 8-cell Li-on batteries.
- Functionality:
- Option 1: The power bank is charged via one of the two Type-C PD ports using a Type-C PD power adapter.
- Option 2: The power bank charges other devices through the two Type-C PD ports.
- Option 3: The power bank is charger using one barrel connector to connect solar pannel.
What would be the best approach, considering the power management ICs or modules?
Thank you in advance!