Part Number: BQ27Z746
Tool/software:
您好,我们用到BQ27Z746在设计一款产品过程中,发现一颗电池放电到了3V以后,静止的时间超过5个小时,SOC仍然显示是100%,然后再充电到截止电压4.4V,这过程中,SOC一直是100%也没有更新,能告诉我是什么原因导致SOC一直不更新吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我不知道怎么上传文件,只能直接粘贴部分GG文件在这里,请帮我看看
"Settings","Protection","Protection Configuration","00","hex"
"Settings","Protection","Enabled Protections A","57","hex"
"Settings","Protection","Enabled Protections B","35","hex"
"Settings","Protection","Enabled Protections C","14","hex"
"Settings","Protection","Enabled Protections D","cc","hex"
"Settings","Permanent Failure","Enabled PF A","01","hex"
"Settings","Permanent Failure","Enabled PF C","00","hex"
"Settings","Batt Sense","Batt Sense Options","00","hex"
"Settings","Batt Sense","Batt Sense Config","00","hex"
"Settings","Batt Sense","RLO Charge Config","0c","hex"
"Settings","Batt Sense","RLO Charge Threshold","75","mA"
"Settings","Batt Sense","Buffer Mode Threshold","2500","mV"
"Settings","Batt Sense","Buffer Mode Delay","1","s"
"Settings","Batt Sense","Buffer Mode Recovery","2900","mV"
"Settings","Batt Sense","Buffer Mode PACK Margin","100","mV"
"Settings","Batt Sense","Transition Config","44","hex"
"Settings","Batt Sense","Transition Delay","250","2us"
"Settings","Batt Sense","Protection Enable Delay","3","ms"
"Settings","Batt Sense","Protection Recovery Delay","5","s"
"Settings","Configuration","Charging Configuration","0000","hex"
"Settings","Configuration","Temperature Enable","01","hex"
"Settings","Configuration","DA Configuration","0410","hex"
"Settings","Configuration","FET Options","0146","hex"
"Settings","Configuration","FET OVRD Time","60","s"
"Settings","Configuration","I2C Gauging Configuration","20","hex"
"Settings","Configuration","I2C Configuration","0028","hex"
"Settings","Configuration","Alt I2C Address","00","hex"
"Settings","Configuration","Alt I2C Addr Chk","00","hex"
"Settings","Configuration","Auth Config","00","hex"
"Settings","Configuration","Power Config","0011","hex"
"Settings","Configuration","GPO Pin Config","00","hex"
"Settings","Configuration","Host Intr Config","00","hex"
"Settings","Configuration","Init Voltage High Set","4500","mV"
"Settings","Configuration","Init Voltage High Clear","4400","mV"
"Settings","Configuration","Init Voltage Low Set","2500","mV"
"Settings","Configuration","Init Voltage Low Clear","2600","mV"
"Settings","Configuration","Init Temperature High Set","60","°C"
"Settings","Configuration","Init Temperature High Clear","55","°C"
"Settings","Configuration","Init Temperature Low Set","0","°C"
"Settings","Configuration","Init Temperature Low Clear","5","°C"
"Settings","Configuration","SOC Delta","1","%"
"Settings","Configuration","SOC Flag Config A","0c8c","hex"
"Settings","Configuration","SOC Flag Config B","8c","hex"
"Settings","Configuration","IT Gauging Configuration","f5de","hex"
"Settings","Configuration","IT Gauging Ext","003b","hex"
"Settings","AFE","ZVCHG Exit Threshold","2000","mV"
"Settings","AFE","ZVCHG PACK Threshold","1500","mV"
"Settings","BTP","Init Discharge Set","150","mAh"
"Settings","BTP","Init Charge Set","175","mAh"
"Settings","BTP","Init Discharge Set RSOC","10","%"
"Settings","BTP","Init Charge Set RSOC","15","%"
"Settings","Lifetimes","Lifetimes Configuration","0000","hex"
"Settings","Lifetimes","Time RSOC Threshold A","95","%"
"Settings","Lifetimes","Time RSOC Threshold B","90","%"
"Settings","Lifetimes","Time RSOC Threshold C","80","%"
"Settings","Lifetimes","Time RSOC Threshold D","50","%"
"Settings","Lifetimes","Time RSOC Threshold E","20","%"
"Settings","Lifetimes","Time RSOC Threshold F","10","%"
"Settings","Lifetimes","Time RSOC Threshold G","5","%"
"Settings","Manufacturing","Mfg Status init","0078","hex"
"Permanent Fail","SUV","Threshold","1800","mV"
"Permanent Fail","SUV","Delay","5","s"
"Permanent Fail","SOV","Threshold","4650","mV"
"Permanent Fail","SOV","Delay","5","s"
"Permanent Fail","CFET","OFF Threshold","5","mA"
"Permanent Fail","CFET","OFF Delay","5","s"
"Permanent Fail","DFET","OFF Threshold","-5","mA"
"Permanent Fail","DFET","OFF Delay","5","s"
"Advanced Charge Algorithm","Temperature Ranges","T1 Temp","0","°C"
"Advanced Charge Algorithm","Temperature Ranges","T2 Temp","10","°C"
"Advanced Charge Algorithm","Temperature Ranges","T5 Temp","20","°C"
"Advanced Charge Algorithm","Temperature Ranges","T6 Temp","25","°C"
"Advanced Charge Algorithm","Temperature Ranges","T3 Temp","45","°C"
"Advanced Charge Algorithm","Temperature Ranges","T4 Temp","55","°C"
"Advanced Charge Algorithm","Temperature Ranges","Hysteresis Temp","1","°C"
"Advanced Charge Algorithm","Low Temp Charging","Current Low","132","mA"
"Advanced Charge Algorithm","Low Temp Charging","Current Med","352","mA"
"Advanced Charge Algorithm","Low Temp Charging","Current High","264","mA"
"Advanced Charge Algorithm","Low Temp Charging","Voltage","4400","mV"
"Advanced Charge Algorithm","Standard Temp Low Charging","Current Low","1980","mA"
"Advanced Charge Algorithm","Standard Temp Low Charging","Current Med","4004","mA"
"Advanced Charge Algorithm","Standard Temp Low Charging","Current High","2992","mA"
"Advanced Charge Algorithm","Standard Temp Low Charging","Voltage","4400","mV"
"Advanced Charge Algorithm","Standard Temp High Charging","Current Low","1980","mA"
"Advanced Charge Algorithm","Standard Temp High Charging","Current Med","4004","mA"
"Advanced Charge Algorithm","Standard Temp High Charging","Current High","2992","mA"
"Advanced Charge Algorithm","Standard Temp High Charging","Voltage","4400","mV"
"Advanced Charge Algorithm","High Temp Charging","Current Low","1012","mA"
"Advanced Charge Algorithm","High Temp Charging","Current Med","1980","mA"
"Advanced Charge Algorithm","High Temp Charging","Current High","1496","mA"
"Advanced Charge Algorithm","High Temp Charging","Voltage","4100","mV"
"Advanced Charge Algorithm","Rec Temp Charging","Current Low","2508","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Current Med","4488","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Current High","3520","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Voltage","4400","mV"
"Advanced Charge Algorithm","Pre-Charging","Current","88","mA"
"Advanced Charge Algorithm","Voltage Range","Precharge Start Voltage","2500","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Low","2900","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Med","3900","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage High","4400","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Hysteresis","0","mV"
"Advanced Charge Algorithm","SoC Range","Charging SoC Med","50","%"
"Advanced Charge Algorithm","SoC Range","Charging SoC High","75","%"
"Advanced Charge Algorithm","SoC Range","Charging SoC Hysteresis","1","%"
"Advanced Charge Algorithm","Degrade Mode 1","Cycle Threshold","50","-"
"Advanced Charge Algorithm","Degrade Mode 1","SOH Threshold","95","%"
"Advanced Charge Algorithm","Degrade Mode 1","Runtime Threshold","8760","h"
"Advanced Charge Algorithm","Degrade Mode 1","High SOC Threshold","8760","h"
"Advanced Charge Algorithm","Degrade Mode 1","High Temp Threshold","8760","h"
"Advanced Charge Algorithm","Degrade Mode 1","High Temp at SOC Threshold","8760","h"
"Advanced Charge Algorithm","Degrade Mode 1","Voltage Degradation","10","mV"
"Advanced Charge Algorithm","Degrade Mode 1","Current Degradation","10","%"
"Advanced Charge Algorithm","Degrade Mode 2","Cycle Threshold","150","-"
"Advanced Charge Algorithm","Degrade Mode 2","SOH Threshold","80","%"
"Advanced Charge Algorithm","Degrade Mode 2","Runtime Threshold","17520","h"
"Advanced Charge Algorithm","Degrade Mode 2","High SOC Threshold","17520","h"
"Advanced Charge Algorithm","Degrade Mode 2","High Temp Threshold","17520","h"
"Advanced Charge Algorithm","Degrade Mode 2","High Temp at SOC Threshold","17520","h"
"Advanced Charge Algorithm","Degrade Mode 2","Voltage Degradation","40","mV"
"Advanced Charge Algorithm","Degrade Mode 2","Current Degradation","20","%"
"Advanced Charge Algorithm","Degrade Mode 3","Cycle Threshold","350","-"
"Advanced Charge Algorithm","Degrade Mode 3","SOH Threshold","60","%"
"Advanced Charge Algorithm","Degrade Mode 3","Runtime Threshold","26280","h"
"Advanced Charge Algorithm","Degrade Mode 3","High SOC Threshold","26280","h"
"Advanced Charge Algorithm","Degrade Mode 3","High Temp Threshold","26280","h"
"Advanced Charge Algorithm","Degrade Mode 3","High Temp at SOC Threshold","26280","h"
"Advanced Charge Algorithm","Degrade Mode 3","Voltage Degradation","70","mV"
"Advanced Charge Algorithm","Degrade Mode 3","Current Degradation","40","%"
"Advanced Charge Algorithm","Degrade Mode","Cycle Count Start Runtime","1","-"
"Advanced Charge Algorithm","Degrade Mode","Runtime Update Interval","10","h"
"Advanced Charge Algorithm","Degrade Mode","Runtime Degrade","180","hours"
"Advanced Charge Algorithm","CS Degrade","Temperature Threshold","50.0","°C"
"Advanced Charge Algorithm","CS Degrade","Voltage Threshold","4200","mV"
"Advanced Charge Algorithm","CS Degrade","Time Interval","150","s"
"Advanced Charge Algorithm","CS Degrade","Delta Voltage","25","mV"
"Advanced Charge Algorithm","CS Degrade","Min CV","3000","mV"
"Advanced Charge Algorithm","Termination Config","Charge Term Taper Current","12","mA"
"Advanced Charge Algorithm","Termination Config","Charge Term Voltage Offset","50","mV"
"Advanced Charge Algorithm","Termination Config","Charge Term Charging Voltage","4480","mV"
"Advanced Charge Algorithm","IR Correction","Averaging Interval","12","s"
"Gas Gauging","Current Thresholds","Dsg Current Threshold","7","mA"
"Gas Gauging","Current Thresholds","Chg Current Threshold","12","mA"
"Gas Gauging","Current Thresholds","Quit Current","5","mA"
"Gas Gauging","Current Thresholds","Dsg Relax Time","60","s"
"Gas Gauging","Current Thresholds","Chg Relax Time","60","s"
"Gas Gauging","Max Load","Max Load Current","-690","mA"
"Gas Gauging","Max Load","Max Load Rsoc","50","%"
"Gas Gauging","Design","Design Capacity mAh","690","mAh"
"Gas Gauging","Design","Design Capacity cWh","2691","cWh"
"Gas Gauging","Design","Design Voltage","3900","mV"
"Gas Gauging","Cycle","Cycle Count Percentage","90","%"
"Gas Gauging","FD","Set Voltage Threshold","3000","mV"
"Gas Gauging","FD","Clear Voltage Threshold","3100","mV"
"Gas Gauging","FD","Set % RSOC Threshold","0","%"
"Gas Gauging","FD","Clear % RSOC Threshold","5","%"
"Gas Gauging","FC","Set Voltage Threshold","4400","mV"
"Gas Gauging","FC","Clear Voltage Threshold","4300","mV"
"Gas Gauging","FC","Set % RSOC Threshold","100","%"
"Gas Gauging","FC","Clear % RSOC Threshold","95","%"
"Gas Gauging","TD","Set Voltage Threshold","3200","mV"
"Gas Gauging","TD","Clear Voltage Threshold","3300","mV"
"Gas Gauging","TD","Set % RSOC Threshold","6","%"
"Gas Gauging","TD","Clear % RSOC Threshold","8","%"
"Gas Gauging","TC","Set Voltage Threshold","4400","mV"
"Gas Gauging","TC","Clear Voltage Threshold","4300","mV"
"Gas Gauging","TC","Set % RSOC Threshold","100","%"
"Gas Gauging","TC","Clear % RSOC Threshold","95","%"
"Gas Gauging","State","Cycle Count","1","-"
"Gas Gauging","State","Qmax Cell 1","767","mAh"
"Gas Gauging","State","Qmax Day","46218","-"
"Gas Gauging","State","Qmax Cycle Count","1","-"
"Gas Gauging","State","Update Status","0e","-"
"Gas Gauging","State","Cell 1 Chg Voltage at EoC","4454","mV"
"Gas Gauging","State","Current at EoC","12","mA"
"Gas Gauging","State","Avg I Last Run","-676","mA"
"Gas Gauging","State","Avg P Last Run","-254","cW"
"Gas Gauging","State","Delta Voltage","5","mV"
"Gas Gauging","State","Temp k","10.00","°C/256mW"
"Gas Gauging","State","Temp a","640","s"
"Gas Gauging","State","Max Avg I Last Run","-702","mA"
"Gas Gauging","State","Max Avg P Last Run","-294","cW"
"Gas Gauging","State","SOH Temp k","1.00","°C/256mW"
"Gas Gauging","State","SOH Temp a","1000","s"
"Gas Gauging","IT Cfg","Load Select","1","-"
“电量监测”,“IT Cfg”,“负载模式”,“1”,“-”
“气体监测”,“IT cfg”,“用户速率-mA”,“0”,“mA”
“Gas Gauging”,“IT Cfg”,“User Rate-cW”,“0”,“cW”
“电量监测”,“IT Cfg”,“预留容量-mAh”,“0”,“mAh”
“电量监测”,“IT cfg”,“储备上限-cWh”,“0”,“cWh”
“气体测量”,“IT Cfg”,“预测环境时间”,“2000”,“s”
“电量监测”,“IT 配置”,“设计电阻”,“661”,“m欧姆”
“气体测量”,“IT cfg”,“Pack Resistance”,“0”,“mOhm”
“电量监测”,“IT 配置”,“系统电阻”,“0”,“mOhm”
“气体监测”,“IT cfg”,“Ra 滤波器”,“80.0”,“%”
“气体测量”,“IT Cfg”,“Ra Max Delta”,“15”,“%”
“气体监测”,“IT cfg”,“电阻参数滤波器”,“65142”,“-”
“气体监测”,“IT cfg”,“靠近 EDV Ra 参数滤波器”,“62184”,“-”
“电量监测”,“IT Cfg”,“Cell 1 互连电阻”,“0”,“2^-10ohm”
“气体监测”,“IT 配置”,“最大电流变化 %”,“10”,“%”
“气体监测”,“IT Cfg”,“电阻更新电压”,“50”,“mV”
“气体监测”,“IT Cfg”,“Qmax Delta”,“5”,“%”
“Gas Gauging”,“IT Cfg”,“Qmax 上限”,“130”,“%”
“电量测量”,“IT 配置”,“周期调整阈值”,“20”,“-”
“电量监测”,“IT 配置”,“周期调整幅度”,“5”,“0.01 %”
“气体监测”,“IT cfg”,“OCV Pred Active T Limit”,“200”,“s”
“气体监测”,“IT cfg”,“OCV Pred Transient T”,“300”,“s”
“气体监测”,“IT cfg”,“OCV Pred 测量时间”,“200”,“s”
“电量监测”,“IT cfg”,“Term voltage”,“16106”,“mV”
“气体监测”、“IT 配置”、“V 项保持时间”、“2”,“s”
“气体监测”,“IT cfg”,“Term Voltage Delta”,“200”,“mV”
“Gas Gauging”,“IT Cfg”,“Max Simulation Iterations”,“50”,“-”
“气体监测”,“IT cfg”,“模拟近端增量”,“250”,“mV”
“气体监测”,“IT 配置”,“快速启动 SOC”,“10”,“%”
“气体监测”,“IT cfg”,“最小电压增量”,“0”,“mV”
“气体测量”,“平滑”,“平滑松弛时间”,“1000”,“s”
“气体监测”,“平滑”,“项平滑起始单元 V Delta”,“150”,“mV”
“气体测量”,“平滑”,“项平滑最终单元 V 增量”,“100”,“mV”
“气体测量”,“平滑”,“项平滑时间”,“20”,“s”
“气体监测”,“SoH”,“SoH 负载率”,“5.0”,“小时率”
Thu Jan 09 11:31:05 GMT+08:00 2025 Device Version Info = 1746_1_05 BQZ Device Name = bq27z746R1 BQZ Firmware Version = 1_05 Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,MaxLoadCurrent,MaxLoadTimeEmty,VoltHiSet,VoltHiClear,VoltLoSet,VoltLoClear,TempHiSet,TempHiClear,TempLoSet,TempLoClear,SOCDeltaSet,BTPDsgSet,BTPChgSet,IntStatus,ChgCurr,ChgVolt,QmaxCC,TermV,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,BattSenseOutput,BattSenseStatus,SafetyAlert 1,SafetyAlert 2,SafetyStat 1,SafetyStat 2,Elapsed Time,PackPinV,CellVolt,CellCurr,CellPower,IntTemp,TS1Temp,TS1Temp,CellTemp,FETTemp,Cell1RawV,CellRawI,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,CompRes1,PackGrid,LStatus,CellGrid1,StateTime,DOD0_1,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,QMax1,QMaxDOD0_1,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,SOH_FC_Q,SOH_FC_E,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,LogRowTime(ms),LogStatus 1,2025-01-09 11:31:11,5.009,0x0054,0,65535,24.4,4446,0,-12,-5,100,0,0,0,65535,-702,0,4500,4400,2500,2600,60,55,0,5,1,150,175,0x00,3520,4400,1,16106,0x00E0,1,0,0x0186,0x0040,0x08,0x0008,0x6A,0x2918,0x0078,0x60,0x00,0x0000,0x0000,0x0000,0x0000,3993776304,4473,4446,0,0,24.4,24.8,-273.2,24.4,-273.2,4446,0,-3,0,0,0,-3,0,0,0,0,0,24.4,24.4,1000,0,1,14,1,71,396,2,0,0,472,767,362,2,29,10.0,640,400,0,0,0x0000,0x0000,0x0000,0x0000,1098,SUCCESS 2,2025-01-09 11:31:16,10.011,0x0054,0,65535,24.3,4446,0,-8,-4,100,0,0,0,65535,-702,0,4500,4400,2500,2600,60,55,0,5,1,150,175,0x00,3520,4400,1,16106,0x00E0,1,0,0x0186,0x0040,0x08,0x0008,0x6A,0x2918,0x0078,0x60,0x00,0x0000,0x0000,0x0000,0x0000,3993776309,4474,4446,0,0,24.3,24.8,-273.2,24.3,-273.2,4446,0,-3,0,0,0,-3,0,0,0,0,0,24.4,24.3,1000,0,1,14,2,0,396,2,0,0,472,767,362,2,29,10.0,640,400,0,0,0x0000,0x0000,0x0000,0x0000,1048,SUCCESS