This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74502H-Q1: Can this part use for 48V 15A supply?

Part Number: LM74502H-Q1
Other Parts Discussed in Thread: LM74800-Q1, LM74700-Q1, LM7480-Q1

Tool/software:

Hi,

      I am rather new to Ideal Diode circuit.   I planning to build one that can be used on 12V, 24V and 48V, each rail can deliver up to 15A.   Mainly, I need it to act as a protection for the power supply, such as Reverse polarity protection, reverse current flow.

      So for such a circuit, is the above controller suited for it?  What will be the suitable FET to use without the use of heatsink?   The EVK seem to be for 12V and 24V and max at 5A, do you have one that works for 48V 15A too?  

Regards

WS