This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Low side mosfet would turn on

Part Number: BQ25703A
Other Parts Discussed in Thread: BQ25703

Tool/software:

Dears,

  The customer used BQ25703 and found that the low side MOSFET would turn on, causing the battery to be pulled down to a protective state. The probability was originally very small, but later in order to control the input voltage to be greater than 12V before it can be turned on. The customer has added input voltage and current limiting circuits, which means that MQ2206 is turned off when the input voltage is below 12V, and only turn on when the input voltage is greater than the set voltage of 12V. When inserting and unplugging Type C twice in a row, there is a high probability that the second time will trigger the phenomenon of low side MOSFET turn on. May I ask when this phenomenon will occur? How to set it up to solve this problem? Thanks.