This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54821: Is the low side MOSFET turned off when EN pin pulled to GND?

Part Number: TPS54821

I would like to know if the low side MOSFET is turned off in the TPS54821 when the EN pin is pulled to GND? The reason I ask is because I would like to use the TPS54821 to convert +12V on the PVIN/VIN pins to a programmable output voltage in the range 3V - 11.5V, but sometimes I would like to apply +12V to the output rail from another voltage source and so during this situation I would like to disable the TPS54821 (ie pull EN pin to GND). This scenario will only work if the low side MOSFET is guaranteed to be turned off when EN low, otherwise the TPS54821 ends up sinking a whole lot of current from the alternative voltage source.