This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: Tell me about the changes in SOH and Ra

Part Number: BQ40Z50-R2

Tool/software:

Hello everyone.

I am experiencing a strange phenomenon in 40Z50 where I have made a mistake in calibration.

Voltage calibration
Battery voltage:16.671V
Pack Voltage: 16.671V
Cell Voltage: 4.066V
Cell Voltage: 4.066V => 0.1V lower than the real Cell voltage of 4.166V.

Repeated 3 cycles of charging and discharging in this state,
SOH: Initial value 99% ⇒ Decreased to 93
Ra changed about 4 times (at around 50% DOD).

Next, 20 cycles of charging/discharging were repeated without changing any settings.
SOH: 93% ⇒ increased to 98
Ra increased from 4 times to 2 times (at around 50% DOD).

Question 1
Why do SOH and Ra change with calibration voltage (Cell) errors?

Question 2
Why do they return to their original values as the number of cycles is repeated?

best regards.