This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSI31P1-Q1: Function of Pins 6 and 7

Part Number: TPSI31P1-Q1


Tool/software:

Hi,

I'm interested in using the TPSI31P1-Q1 in a 800V pre-charge design.

In the device datasheet the Pins 6 and 7 are marked as NC whereas in the EVM User's Guide these pins are named with PC50 and PC100, without further description of thier function:

Is there any function behind these two pins, as stated in the EVM?

When will the TPSI31P1-Q1 go into production?

Best regards
Ludwig