Tool/software:
Dear forum
I want to use a TPS22994 to switch the outputs of four TPS6223* converters.
The TPS6223* seems to be optimised for a 4.7 uF output capacitor, even tough 2 - 15 uF should be ok (datasheet, page 13, section 9.2.2.1).
On the other hand, the TPS22994 calls for an input capacitor of 1 uF and an output capacitor of one tenth of this value (datasheet, page 35, section 11.1).
What is the better strategy in this case?
- Try to place the buck converters as close as possible to the load switch and use a single 4.7 uF capacitor. Use 470 nF as output capacitor for the load switch.
- Use 4.7 uF at the buck converter output. Use an additional 1 uF at the load switch input. Use 100 nF at the load switch output.
- Use 4.7 uF at the buck converter output. Use an additional 1 uF at the load switch input. Use 560 nF at the load switch output.
- Use 3.3 uF at the buck converter output. Use an additional 1.5 uF at the load switch input (totalling 4.8 uF). Use 150 nF at the load switch output.
- Use 3.3 uF at the buck converter output. Use an additional 1.5 uF at the load switch input (totalling 4.8 uF). Use 470 nF at the load switch output.
- Others?
Thank you in advance, Enpa