This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: I want to make ±24V output with INPUT12V.

Part Number: TPS61170

Tool/software:

I was looking at the E2E forum and found the following schematic.
I would like to configure INPUT: 12V, OUTPUT: 24V, -24V.

The output current is about 50mA.
Please let me know if there are any changes I should make.

0358.TPS61170 24Vo.pdf