This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS631013: IC substitute material inquiry

Part Number: TPS631013
Other Parts Discussed in Thread: TPS55289

Tool/software:

Hi Team

Do we currently have a Buck-Boost IC that can meet this need?
In addition, customers have requirements that the output voltage (primary), current (primary), and temperature (secondary) status must be known through the "communication function"

A. The input is about 4.2V, the output is 3.8V, and the output current is 3A.
B. The input is about 4.2V, the output is 4.6V, and the output current is 3A.

Thanks

Boyan