Tool/software:
Hi,
I'm working on simulating this part in LTSpice, but after I create my circuit and go to run it, I get a series of errors. Can someone help clear these for me.
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I'm working on simulating this part in LTSpice, but after I create my circuit and go to run it, I get a series of errors. Can someone help clear these for me.
thank you
Hi Michael,
This is difficult to troubleshoot on my end because we do not use LTSpice, and our models are made to run in PSPICE. I will take a look at the model to see if the errors you are seeing make sense for PSPICE, but for LTSpice I won't be able to help much.
Regards,
Nick
Hi Michael,
I think the issue is that the model expects an external parameter V_out, and all 3 of these issues stem from V_out not being defined. The screenshot is the test bench that the model comes with.
I was able to make the model work by adding the parameter to the internal parameter list. On line 123 in the library file, add the V_out parameter with the output voltage setting you are looking for. Note that it's a single space between the vref parameter and no comma.
This should at least resolve the issues that you posted, but this won't guarantee that the model will work with LTSpice.
Regards,
Nick