Tool/software:
Good afternoon. I am having trouble with learning cycle, we are stuck at Learned Status 5 and can not progress to 6 after several discharge cycles.
The cells are 4S10P LG M50LT 21700 5,000 mAh
I Since resistor is 0.125Ω therefor the max current is 1,000 mA as we require high resolution current sensing for this low power IoT device.
Braking this down is steps: -
Learn-11-12-24.gg.csv7140.Learn Log discharge11.5v.log
Screen shot taken after a re-charge: -
Best Regards
Anthony