This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: BQ27Z746_Low temperature optimization

Part Number: BQ27Z746
Other Parts Discussed in Thread: GPCRB

Tool/software:

Hi ti team
I am using BQ27Z746 for low temperature optimization,attached is the optimization file provided by TI, which I used for testing. However, I found that the SOC accuracy was very high at 1A low temperature discharge, but the SOC accuracy of 2A low temperature discharge was significantly worse.Is there any way to improve the SOC accuracy of 2A low temperature discharge?

1346.1A@-20℃.xlsx8203.2A@-20℃.xlsx

4073.Send to TI (GPCRB)V2-21700-1s2p-9600-PANASONIC_report.zip