Tool/software:
Hi Team
1. Does the BQ25185 accept 12V DC input for charging?
2. Can the system voltage (SYS) be fixed at 5V output?
3. When charging is disconnected, will the system voltage maintain a 5V output?
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team
1. Does the BQ25185 accept 12V DC input for charging?
2. Can the system voltage (SYS) be fixed at 5V output?
3. When charging is disconnected, will the system voltage maintain a 5V output?
Frank
Hello Frank,
1. Yes, the BQ25185 input voltage operating range is 3 - 18V. However, thermal dissipation at a 12V input should be considered a limiting factor for charge and load current. For example, with a 12V input and a 4V battery, the charger will dissipate 0.8W for every 100mA of current.
2. No, the system voltage (VSYS) is regulated to 4.5V when a valid input source is present.
3. No, when the input source is removed, VSYS will just be the the battery voltage. More details about SYS regulation can be found in section 8.3.5 of the datasheet.
Please let me know if you have any further questions.
Best regards,
Alec
In Section 7.5 "Electrical Characteristics (continued)," it states that when the battery voltage is less than 3.6V, Vsys = 3.8V. I don't quite understand this.
Does it mean that as long as the battery voltage is greater than 3.6V, Vsys will output 4.5V?
Frank
Hello Frank,
When an input source is connected and the ILIM/VSET pin is configured for a VBATREG higher than 4.3V, the system voltage (VSYS) is regulated in battery tracking mode.
In battery tracking mode:
Best regards,
Alec