This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS785-Q1: Fixed mode IC model for TPS78533QKVURQ1

Part Number: TPS785-Q1

Tool/software:

Hi 

can you share the fixed mode IC model for part number TPS78533QKVURQ1 (5 pin configuration)

below is our application design

I have already taken spice model from website but it has 6 pins - when used this 6 pin model in simulation with fixed mode - not getting desired output voltage (as model works for adjustable mode with Feedback resistors connected and not providing desired output for Fixed mode when FB is NC)