Tool/software:
Hi,
I´m going to introduce the component TPS26400 in our design.
I have a doubt about these pins UVLO, OVP, and SHDN regarding the reverse input supply protection.
In datasheet it is specified that this IC has integrated reverse input polarity protection down to –42V, but in the point 7.1 "Absolute Maximum Ratings" it is specified these values for that pins:
They don´t accept negative values. Only IN and OUT pins.
I have these schematic:
Will I have problems with that pins?, or they are protected too against reverse input supply?