Part Number: UCC28056
Tool/software:
Good morning. We are developing a PFC implementing TI's UCC28056 controller to power an inverter that drives a brushless DC motor.
Looking at the voltage at the output of the PFC (aka the bus voltage Vbus) we have noticed fluctuations in the value of Vbus due to small load variations caused by the speed control of the motor.
To our understanding in order to attenuate this phenomenon we can either increase the output capacitance of the PFC (which we prefer not to, as it increases the cost of the system) or increase the bandwidth of the voltage compensation loop, while keeping the same phase margin at the expense of more THD in the input current.
Since we have some margin on the specifications of THD we are considering this solution.
Normally, the maximum bandwidth of the voltage loop of a PFC must remain below 20Hz so that the compensation network effectively attenuates the ripple at twice the line frequency, which causes third-harmonic distortion of the input current.
What we would like to know is what happens if we increase the bandwidth beyond 20Hz and if there exists a procedure to maximize the bandwidth of a PFC in this condition where the ripple on the compensation network becomes non-negligibile