This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC77: TLC7705QD part behavior at Full Temperature Range

Part Number: TLC77

Tool/software:

Greetings

Currently we are testing Pat# TLC7705QD (non military grade )Power supply monitor and need to clarify the following

In the switching characteristics table, the Delay Time is specified at 25C with limits "min=1.1ms" and "max=4.2ms", however on the test condition indicates "Ta= Full Range" What is the expected behavior of the device as it approaches the temperature limit?"