Tool/software:
I am trying to run a worst case analysis on the circuit using this part and wanted to know what tolerances I should include in my calculations to accurately capture the full range of the regulated voltage. Right now I am just using the variation of the Vadj 1.174V-1.246V. This is the variation from the datasheet which is specified as over the full temperature range, but it’s unclear if this includes radiation or aging. Should I be considering anything from the internal error amplifier like input offset voltage, input bias current, and input offset current or are these small enough to be considered negligible?