Other Parts Discussed in Thread: TPSM83100
Tool/software:
Hi,
I need a buck boost IC with low noise and small size(LOW BOM count as well). I don't want to use BGA with very fine pitch like TPS631010. The inductor size should be very small as well. I have not much space available on the board
The input is single cell lipo battery 3 to 4.2V. I need 3V and 1 to 1.5A output.
Can you recommend any IC?
Thanks