Part Number: UCC2897A
Other Parts Discussed in Thread: TL431, UCC2891, , TPS28225
Tool/software:
Hello,
I am designing a fixed-frequency active clamp flyback converter that do not require the secondary ground to be isolated from the primary. As a result, compensating the loop with an optocoupler and TL431, as typically suggested in references, is not an optimal solution for my application. Are there any reference materials available for closing the loop when using this IC or any member of the UCC2891/2/3/4/7 family without an optocoupler?
Additionally, since isolation is not required, could you recommend a general-purpose current-mode controller with complementary outputs and programmable dead time as an alternative to the UCC289x family for implementing a fixed-frequency ACF?
Thanks,
Ajmal