This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV704: Application issues

Part Number: TLV704

Tool/software:

Hi

Does the TLV704 LDO have a static current and input voltage curve similar to the one shown in Figure 1? The output voltage is 3.3V, and the input voltage needs to start from 0V. The relationship between static current and input voltage on the datasheet shows that the input voltage starts from 3V, as shown in Figure 2; Does TI have an LDO that can maintain its own static current at around 3-10uA when Vin ≤ Vout+Vdo?