Tool/software:
We were using it to step down 12V to 5V.
In another product, we would like to use it to step down 24V to 5V.
Questions
1) Are there any points I should be careful about regarding the COMP terminal(7pin)?
I think the COMP terminal is an output terminal, but will the output voltage of the COMP terminal change if 24V is input?
I'm concerned about the withstand voltage of the element connected to the COMP terminal.
2) Other than the voltage resistance of the elements to be connected to the input terminal, I would like some advice on any precautions to take when changing from a 12V input to a 24V input.