This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: Omitting Reverse Battery Protection DGATE, Using Load Disconnect Switch Control HGATE

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM74800-Q1, LM74502-Q1, LM7481-Q1,

Tool/software:

Hello,

Referring to the image from the datasheet below.

I want to omit Q1, the FET relating to ideal diode functionality.
But use Q2, the FET relating to load switch functionality.
Possibly in a back to back configuration, for reverse voltage protection.

My goal is to provide reverse voltage protection, but to allow reverse current flow.
It would be used on a battery interface, where the battery would be both charged and discharged.

What is the recommended approach?

If Pin A and Pin C are connected together, at the same voltage, and Q1 is not populated, would Q2 operate normally?

Thanks

EDIT:  I don't want to use the LM74801-Q1 variation, because i will be using the LM74800-Q1 elsewhere in my design.

 9.2