Tool/software:
Hi Sir,
For Strobe function setting on the Register(0x01), may I know need to set the bit-1 = 1 and the bit-0 = 1, is it right? or set the bit-2 = 1 or bit-3 = 1?
To meet the Register(0x02) Flash Time-out duration width function, to set the Register(0x01) bit-2 = 1 and bit-3 = 1, is it right? or set the bit-2 = 1 and bit-3 = 0?
schematics: