Tool/software:
Hi team,
I am testing using a TPS1HC100EVM as a PWM controller to drive an LED strip to avoid using a large external MOSFET. The LED strip would consume about 1A at 12V, which I believe is within the capabilities of this HSS. While I currently don't have an LED strip to act as the load yet, I am testing PWM'ing the EN pin to vary the output voltage of the EVM, but no matter what I set the duty to, it outputs 12V until I get below ~25% duty. At that point, the output voltage slightly decreases but the lowest I've seen is 10.6V. The switching frequency is 490Hz, which should be acceptable according to the datasheet.
Is there something else that I need to do other than just PWM'ing the EN pin? I confirmed the PWM signal being sent to EN is good by measuring the frequency and voltage being output with a multimeter, which were as expected. Max voltage when I set it to 100% duty is ~4.7V, 50% duty shows ~2.4V, and so on. There is no load attached at this time while I wait for the LED strips to come in.