This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Synchronous Rectification as H-Brdige

Part Number: UCC28950
Other Parts Discussed in Thread: UCC28951

Tool/software:

Hi,

I am wondering if it is possible to connect the synchronous rectifier as an H-Bridge Configuration using the E and F PWM signals generated from the chip. My immediate thought is no because of the E and F timing signals are overlapping during switching cycles and would thus cause shoot through failures. Is that thinking correct? Is there another way to utilize the controller generated PWM signals to complete this?

I found this article and was wondering if it was possible w/ the UCC28950 or is it only possible with a digital controller solution?

https://www.ti.com/lit/an/slyt835/slyt835.pdf?ts=1736954809624&ref_url=https%253A%252F%252Fwww.google.com%252F

Regards,

-Noah