This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI: TINA

Part Number: TINA-TI


Tool/software:

  • We need to design PCB of 10kW power supply (0-30V DC (step maximum 10mV), 0-340A (step maximum 100mA)) working as a voltage and current source with feedback loop for stable voltage and current. Otherwise, it should also work as a sinus generator (0V (minimum level) up to 30V (maximum level)) for frequencies 10uHz- 1MHz. The entire power supply / generator should be powered from 400V AC (5 wires: L1, L2, L3, N, PE), should be controlled via 1Gbit Ethernet and should be designed for standard rack package: 3U, 1000 mm