Tool/software:
I worked on this quite a while without success. Please take a look and make your suggestions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I worked on this quite a while without success. Please take a look and make your suggestions.
Hi Pete,
we will look into this and come back till mid of next week.
Best regards,
Stefan
Hi Pete,
Thanks a lot for your patience.
I have run your simulation and got the same convergence error.
It might be related to the MOSFET models you are using.
I also noticed you are using a sense resistor of 500mOhm, which is rather high. (R8)
I have run the simulation with ideal MOSFETs. Here the simulation runs fine.
The simulation file is attached below.
Please let me know if you can work with this model, or if there are additional questions.
Best regards,
Niklas
I am trying to design a 24V large capacitance 100ma charger. I did one and successfully modeled it in Analog Devices Spice. We want to take advantage of the synchronous regulation to reduce the difference that a diode rectified circuit has. The low current requirement is why the sense resistor and inductor are so large. I ran the AD feedback loop not with voltage sense but with average current sensed off the sense resistor. Is there a more stable actual FET we could use? The AD sim used a MAX51597 with an IRFZ44N and sims ran quickly. We are fabricating that in case I cannot demonstrate this using actual FET models and not voltage-controlled switches. The large capacitance shares with a low current PS and allows very high, infrequent large pulse loads. It is a retrofit option for the customer's existing system.
Hi Pete,
Thanks for the clarification.
Unfortunately, I am no MOSFET expert, so I cannot recommend a specific part, nor can I say which FETs will run fine within the simulation and which ones will not.
I would recommend to check if your simulation runs fine with ideal MOSFETs first, so we can clarify that the MOSFETs are cause the convergence error.
Instead of switching to other MOSFET parts, it might also be possible to achieve convergence by adjusting the simulation setting. (e.g. changing step size and convergence parameters)
More details on this can be found here:
e2e.ti.com/.../lm5118-pspice-reference-simulation-not-converging
Best regards,
Niklas